Skip to content
Menu Close
Home > News > How to Hook up a Load Bank to a Generator

How to Hook up a Load Bank to a Generator

Last Updated on April 12, 2023

Backup power generators are increasingly valuable for construction sites, hospitals, military sites and industries that need security during energy outages. Generator load bank testing ensures that these generators can power machinery for an entire system during an emergency outage.

Trystar can help you learn how a generator load bank works, how to connect the two devices and where to find quality load banks and generators.

WHAT IS A GENERATOR LOAD BANK AND WHY IS IT IMPORTANT?

A load bank is a self-contained device that simulates a real-world load to test how much electrical energy a generator can handle. The operator can double-check that the generator will function in an emergency. The test also exercises the generator to promote activity and reduce decay. Regular testing can also prevent wet stacking on diesel generators so that soot does not build within the system.

Regularly testing a generator is often a regulatory requirement from the National Fire Protection Association (NFPA) regulation 110 (NFPA 110-2019) and the National Electric Code (NEC) 700. Any facility requiring a level 1 emergency power supply system (EPSS) to prevent loss or harm to human life must regularly test its systems. A level 2 EPSS that does not protect human life also needs testing since these are mission-critical facilities.

HOW OFTEN SHOULD YOU TEST A LOAD BANK?

There are specific federal government requirements that explain how often you need to test a generator depending on the EPSS classification, the minimum number of system uptime hours and the number of seconds it takes for the generator to activate.

For example, hospitals or health care facilities with generators that power life-saving equipment require monthly 30 minute tests and tests up to four hours every three years. It’s often necessary to test a diesel generator with a light load to prevent wet stacking more frequently than once a month.

HOW TO CONNECT A LOAD BANK WITH A GENERATOR

Depending on the generator’s function, there are several distinct methods for hooking up a load bank to a generator. The three main approaches include:

  • Manual transfer switch: The operator connects the generator and the load bank at test time.
  • Automatic connection: The load bank has a circuit breaker that connects the bank and the generator. During the load test, the load bank turns off with a signal from the automatic transfer switch and removes the load from the power generator.
  • Permanent connection: The load bank has a permanent link to the generator so that it senses the building load and performs the test on its own automatically.

LEARN MORE ABOUT GENERATOR AND LOAD BANK SOLUTIONS

Are you interested in finding a generator docking station or load bank for your project? Trystar is here to help. We offer a wide selection of generator docking stations and load banks for you to browse. We offer cutting-edge technology for energy solutions and personalized customer service.

Reach out to us on our quick contact form, or give us a call at 507-248-7475 for personalized information so you can find the perfect fit for your next energy project.

Continue Reading

Blog

Power Reliability In Data Centers: Best Practices For 2025

Blog

Examples Of Successful Emergency Power Strategies Within Data Centers

Company News

Minnesota Army National Guard Awards Trystar Team Members

We Are Here
To Help

Our team is here to support you and solve your power challenges. Connect with our responsive experts today to learn about our customized power solutions and products.

Site Feedback
Close
Close