Skip to content
Menu Close
Home > News > Main Use of Transformers in Power Supply

Main Use of Transformers in Power Supply

Last Updated on April 12, 2023

Where you use alternating current (AC) electrical energy, you may notice the use of transformers. In direct current (DC) systems, industrial power supplies are used to transform AC voltage into low DC voltage.  Transformers, on the other hand, convert AC voltage to AC voltage or current without impacting power.

Transformers are made from an iron core. On the high voltage side of the core, the coil is wrapped many times, and on the lower voltage side of the transformer, the coil is wrapped fewer times. As electricity enters the coil on one side, it induces a magnetic field that produces a higher or lower voltage in the other coil.

WHAT IS THE FUNCTION OF A TRANSFORMER?

Transformers can decrease or increase the voltage, sometimes known as stepping down or stepping up the voltage. Using a transformer can help make the right power accessible to us when we need it.

The purpose of using a transformer in power supply is to make electrical power accessible as it travels from a power utility to an office, home, worksite or other location. Energy is lost when it travels along transmission wires from a power plant to a customer. Utilities use a very high voltage to lose less energy.

Different types of transformers are used along the journey. When electricity travels from a power plant, transformers step up the voltage to allow the electricity to travel efficiently. As it leaves the power plant, electricity may be stepped up to thousands of volts to make its journey. Electricity eventually reaches transmission stations, where transformers and control equipment lower the voltage to safer levels. As the electricity travels along transmission lines, it is further reduced by the transformers on power poles.

Another type of transformer steps down the electricity to 120 V when it enters your home or office. At 120 V, the electricity can be used to power some devices and electrical outlets. You may also use an adapter to convert to DC for some devices, like computers.

WHY DO WE NEED TRANSFORMERS?

Using a transformer allows electricity to be usable and to travel over long distances. This means fewer power plants can economically deliver electricity to a wide range of customers safely without losing much energy. Transformers also ensure the power entering your home is safe for your light bulbs and outlets.

HOW TRYSTAR CAN HELP

If you need energy and power supply at your worksite, Trystar can help with generator docking stations, portable power and other solutions. Whether your organization needs a reliable backup power source to keep mission-critical operations going or you need temporary power for remote sites, we have you covered.

Hospitalsconstruction sitesdisaster response organizations and other companies turn to us when a lot is riding on a power source because we provide efficient and dependable solutions. Our commitment to safety and integrity allows us to focus on our customers’ success. Get in touch with our team today to learn how we can help you.

Continue Reading

Blog

Power Reliability In Data Centers: Best Practices For 2025

Blog

Examples Of Successful Emergency Power Strategies Within Data Centers

Company News

Minnesota Army National Guard Awards Trystar Team Members

We Are Here
To Help

Our team is here to support you and solve your power challenges. Connect with our responsive experts today to learn about our customized power solutions and products.

Site Feedback
Close
Close