Updated and re-published August 20, 2026.
Growing electrical demand, aging grid infrastructure, severe weather, utility capacity constraints, and increasingly power-intensive operations are changing how organizations approach power resiliency. For facilities where downtime carries significant operational or financial consequences, relying exclusively on utility power may no longer provide the flexibility required to support future growth. Microgrids can provide another layer within a broader resiliency strategy by coordinating local generation, energy storage, controls, and critical loads. Depending on the application, they can help facilities maintain critical operations during utility interruptions, manage peak demand, integrate distributed energy resources, and support expanding electrical loads.
But what exactly are microgrids, and how do they work? In this post, we’ll step into the world of microgrids … providing a snapshot of their definition, components, and benefits.
What Are The Main Components Of A Microgrid?
At its core, a microgrid is simply a localized group of electricity sources and loads which are operating together as a single entity. It may be connected to the main electrical grid, but it is also fully capable of functioning independently. Unlike the main electrical grid and centralized power systems which distribute electricity (from large power plants) over long distances, these decentralized grids provide energy on a smaller scale and serve such localized communities as small cities and towns, campuses, military bases, and industrial complexes.
A typical microgrid includes a means of power generation, an energy storage system, a control system, switchgear / protection devices, and the load.
One of the defining features of microgrids is their ability to integrate renewable energy sources such as solar and wind power. Smart inverters and power electronics have contributed to recent advancements in renewable energy technologies to improve efficiencies, reliability, and cost-effectiveness.

independent energy system with power distribution.

and providing power to the load (facility).
Power Generation
Power generation within a microgrid can include a combination of distributed energy resources such as solar, wind, natural gas generators, and other onsite generation technologies depending on the application and operating requirements. Such distributed energy systems can also be interconnected with the main utility grid, as in the example illustration above and the photo to the left. This type of hybrid system leverages the strengths of both centralized and decentralized infrastructure; enabling seamless transition between grid-connected and islanded modes of operation. Bi-directional power flow control, demand response, and grid services enable microgrids to provide value to both grid operators and end-users.
Energy Storage Systems
Energy storage plays a critical role in microgrid operation, providing power resilience and grid support. Battery Energy Storage Systems (BESS) can store energy for use during peak demand, utility interruptions, or periods when onsite generation cannot fully support the load. Depending on system design, BESS can also support load shifting, frequency regulation, grid stability, and the transition between grid-connected and islanded operation. Advances in battery technologies continue to enhance increased energy density, efficiency, and battery cycle life (number of charges/discharges before losing performance).
Control System
At the heart of every microgrid is its control system, which manages the flow of electricity … balancing supply and demand, as well as ensuring the stability and reliability of the localized energy network. Advances in control systems include real-time monitoring, predictive analytics, and adapting to dynamic grid conditions. Advanced microgrid controls can also coordinate generation, energy storage, utility power, and critical loads while determining when resources should operate in grid-connected or islanded modes.

Switchgear & Protection Devices
Switchgear and protective devices help manage, protect, and isolate portions of the electrical system, including supporting the safe separation of a microgrid from the utility grid when required for islanded operation. Additionally, they protect against voltage fluctuations and other power anomalies.
Critical Loads
The electrical equipment systems served by the microgrid represent its load. During islanded operation, available generation and stored energy may be prioritized to support designated critical loads while less-essential loads are reduced or shed.
Benefits Of Microgrids
Decentralized grids represent a paradigm shift in the way that electricity is generated, distributed, and consumed. That said, microgrids do offer several advantages:
- Enhanced Power Resiliency:
By operating independently from the main grid, properly designed microgrids can maintain power to designated loads during utility grid outages caused by severe weather, natural disasters, or cyber attacks. - Increased Renewable Integration:
Microgrids facilitate the integration of renewable energy sources by providing a platform for electrical power generation, distribution, and energy storage … thus reducing the reliance on fossil fuels and lowering greenhouse gas emissions.
- Energy Cost Savings:
Depending on utility rates, operating strategy, available generation, and energy storage capabilities, microgrids may help reduce energy costs through peak-demand management, load shifting, and optimized use of onsite resources. - Grid Support & Stability:
Microgrids can enhance the stability of the main utility grid by providing ancillary services such as peak shaving and voltage regulation. Depending on the utility, market, and applicable program, microgrids may also enable facilities to participate in demand-response or other grid-support programs by reducing demand, managing onsite resources, or providing other ancillary services.

Conclusion
Ongoing advancements in power resiliency and power transition technology are driving the transformation of energy. By enabling decentralized, resilient, and sustainable energy systems, microgrids have the potential to play a vital role in the transition to a more sustainable and secure energy future. Renewable power integration, energy storage, advanced control systems, and grid connectivity … that future is here.
Microgrids … and Trystar … are poised to play a pivotal role in shaping the future of energy. Join the microgrid conversation … ask us how we can partner with you in microgrid opportunities!