Our team is here to support you and solve your power challenges. Connect with our responsive experts today to learn about our customized power solutions and products.

Entertainment / Events
Entertainment Style Transformer

The Trystar Entertainment Transformer is protected by a hefty powder coated cage that can be customized with your company colors. And talk about portability: this unit features lifting points, fork pockets and lockable casters, making it easily transportable for any entertainment application.
Power Distribution Panel

Trystar’s UL Listed Power Distribution Panel is equipped with lifting hooks and fork pockets to help you place it into position. These units are built tough and will stand up to heavy rental and industrial use, and can support temporary power needs at events. The Power Distribution Panels feature a hard bus rather than internal cables and offer extra space for additional breakers if you need them.
Power Distribution Panel

The Trystar Power Distribution Panel is built like a tank, from its stainless steel or aluminum enclosure to its heavy duty roll cage. All the components are top of the line. Over the years it has been tested by hard rental and industrial usage, and it has passed with flying colors.
RV Panel

The Trystar RV Panel is built like a tank, from its stainless steel or aluminum enclosure to its heavy duty roll cage. All the components are top of the line. Over the years it has been tested by hard rental and industrial usage, and it has passed with flying colors
Tuff Box

The Trystar Tuff Box is legendary for its rugged simplicity and durability. With OSHA approval, the Trystar Tuff Box has proven itself on countless entertainment and event sites, where it is valued for its lightweight, bulletproof design. Tough enough for the rental and industrial markets, our Tuff Box is one less thing to worry about.
GridPak

Trystar’s new GridPak is a portable power solution that generates clean, reliable energy with zero CO2 emissions. Since it works on solar energy and battery energy storage, there’s no need to transport fuel to it on a regular basis. Simple technology makes it one of the most reliable temporary power solutions on the market.
Quad Box Stringer

This handy stringer was designed by our engineers to work hard and never come apart. It consists of three rubber outlet boxes which run on three independent circuits. The receptacles within each box are available in GFCI or Edison-style duplex, or a combination of the two.
Spider Box

The Trystar Spider Box is legendary for its rugged simplicity and durability. With OSHA approval, the Trystar Spider Box has proven itself on countless entertainment and event sites, where it is valued for its lightweight, bulletproof design. Tough enough for the rental and industrial markets, our Spider Box is one less thing to worry about.
Power Distribution Panel

The Trystar Power Distribution Panel is built like a tank, from its stainless steel or aluminum enclosure to its heavy duty roll cage. All the components are top of the line. Over the years it has been tested by hard rental and industrial usage, and it has passed with flying colors.
Portable EV Charger

The Trystar Portable Electric Vehicle (EV) Charger is an innovative solution designed to provide convenient and reliable charging for electric vehicles on the go, eliminating the need for charging facilities at your event. This compact and versatile charger is specifically developed for the rental market in mind, catering to the growing demand for mobile and portable power solutions. The charger’s compatibility with mobile power solutions ensures that EV owners can access charging facilities even in areas where fixed infrastructure may be limited.
4/0 Power Cable

Trystar Power Cable is designed to carry the maximum amount of power across the greatest distances on site. It is built to true AWG standards and complies with multiple listing agency requirements. We apply an inner insulation layer in a contrasting color designed to alert you to cuts, nicks and excessive wear on the outer insulation jacket.
6/4 Multi Conductor Spider Box Cable

These multi-conductor, plug and play cables are very user-friendly and can reduce the number of cables needed on a job site. Trystar Spider Box cables are expertly assembled and factory tested to ensure they work out of the box. Tough enough for the most demanding conditions, they have proven themselves in events and entertainment rental applications.
⅖ Banded Power Cable

Trystar Banded Cable has been tested and proven at huge events such as the Bonaroo musical festival, the Ryder Cup and the Super Bowl. It has withstood extreme cold, withering heat, heavy rain and direct sunlight. It features an internal insulation layer in a high contrast color that is designed to pinpoint any damage or wear to the outer insulation jacket. This cable is a proven winner, and is listed for both indoor and outdoor use.
Entertainment and special events — such as concerts, festivals, theater performances, sporting events and more — have unique power requirements. These events are often temporary setups that need portable, reliable power sources to work for several hours or days. These power solutions need to support many kinds of equipment, from microphones to speakers to lighting.
Whether your event is small or large, Trystar can provide temporary power for occasions of all kinds. Our products easily and effectively distribute power to support your equipment throughout the event.
Are you holding an event with a bounce house or other similar inflatable amusement devices? We offer Inflatable Party Packages that will easily power your bounce house inflation equipment.
Special Event Power Solutions at Trystar
Trystar has cables, panels, transformers and more for entertainment/event applications. We can customize your productswith your company’s logos and colors so the equipment will fit your branding.

Boxes and Panels
Large-scale events such as concerts will require more than power strips and extension cords to power the stage lighting, sound system and other equipment. Power distribution panels can power all of these components, and you can control individual circuits from the panel.
Our box and panel equipment is available in many sizes and configurations, so you can pick a style that fits your needs. We offer:
Transformers
Some event venues may have a power supply line that doesn’t suit the equipment’s voltage requirements. A transformer will connect the source and equipment to make them compatible, allowing everything to run off a reliable power source.
We have two transformer styles available — dolly style and cage style — that are both portable and durable to get the job done anywhere power is required.
Portable ATS
For entertainment/event performances, the show must go on at all costs, so coordinators need backup plans in case of unreliable power connections or outages. Connecting your audio and visual equipment to a portable generator may be sufficient in some cases, and using a portable automatic transfer switch (ATS) is the best method. The temporary ATS transfers the power from the main source to the generator efficiently so you can maintain your power connection. This method is also safer than extension cords.
Our portable ATS is a durable unit that provides backup power for critical operations. This solution is often used as a temporary fix when the permanent ATS fails.
Entertainment Cable
Entertainment systems require the right cable to establish secure connections. We have many types of cables for events that have worked successfully in large-scale venues. For the entertainment industry, we recommend the stage and lighting cable, which is made for indoor and outdoor use to withstand the elements. It also has internal insulation and a high-contrast cover.

Major Events Trystar Has Powered
Trystar has provided temporary power for events across the United States, so our equipment is tested and proven for reliability in critical applications. We have powered these and many other events: